Auxiliaries NII_Z_1: Check Auxiliary Wiring and Insulation
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Visually check external and internal wiring and insulation of control and indication auxiliaries. |
|
Goal |
Verify electrical continuity of auxiliary circuits and contact robustness. |
|
Frequency |
Refer to Recommended Frequency for the Routine End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
Flat screwdriver, 3 mm |
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Disconnected |
Checking Terminal Block and Connector Wiring
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK
Use a properly rated voltage sensing device to confirm
that the PTE voltage measurement input is
de-energized (V1, V2, V3 on UC4 terminal
block, VN on UC3 terminal
block).
Failure to follow these instructions will result in death or serious injury.
|
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Remove the auxiliary terminal shield from a drawout device, if present. |
|
|
2 |
Check that the external wiring is connected securely in the terminals. |
If the connection is loose, replace the terminal blocks (refer to MasterPacT MTZ1/MTZ2/MTZ3 - Auxiliary Terminals - Instruction Sheet). Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. |
|
3 |
Visually check the insulation of the external wiring. |
If the wire insulation is cracked or damaged, replace the wires. |
|
4 |
Check the terminal blocks for warping, damage, or change in color indicating abnormal temperature rise. |
If there is a change in color, replace the terminal blocks (refer to MasterPacT MTZ1/MTZ2/MTZ3 - Auxiliary Terminals - Instruction Sheet). |
|
5 |
For a MasterPacT MTZ2/MTZ3 drawout device, remove the terminal block identification plate. |
|
|
6 |
Check the connection and wire insulation between the two parts of the terminal blocks. |
If the connection is loose or the wire insulation is cracked or damaged, replace the terminal blocks (refer to MasterPacT MTZ1/MTZ2/MTZ3 - Auxiliary Terminals - Instruction Sheet). |
|
7 |
Check the mounting of connectors on the auxiliary crossbar. |
|
|
8 |
For a device with ULP port module, refer to Checking Connection on the Optional ULP Port Module. For a device with EIFE interface, refer to Checking Connection on the Optional EIFE Interface. |
|
|
9 |
Put the terminal block identification plate and the auxiliary terminal shield back in place. |
Checking Connections on the Optional ULP Port Module
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check the connection of the 24 Vdc power supply on the ULP port module. |
|
|
2 |
Check the connection of the ULP cords on the ULP port module. |
If a plug clip on an RJ45 connector is damaged, replace the ULP cord. Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. |
|
3 |
Check the ULP cord insulation. |
If the insulation is cracked or damaged, replace the ULP cord. Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. |
Checking Connections on the Optional EIFE Interface
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check the connection of the ULP cord on the EIFE interface. |
Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. |
|
2 |
Check the connections of the Ethernet cables on the EIFE interface. |
If a plug clip on an RJ45 connector is damaged, replace the Ethernet cable. |
|
3 |
Check the Ethernet cable insulation. |
If the insulation is cracked or damaged, replace the Ethernet cable. |
DANGER