Chassis Locking NII_Z_2: Operate Chassis Padlocking System
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check the locking and unlocking of the chassis with padlocks in disconnected position or in any position, according to the chassis locking configuration. |
|
Goal |
Verify that the chassis padlocking system correctly operates. |
|
Frequency |
Refer to Recommended Frequency for the Routine End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
N/A |
N/A |
N/A |
|
Drawout |
Open |
Discharged |
Disconnected |
Determining the Chassis Locking Configuration
The MasterPacT MTZ drawout devices offer two chassis locking possibilities with padlocks:
-
In disconnected position.
-
In any position (disconnected, test, or connected).
To determine the chassis locking possibility, move the device to the connected or test position:
-
If you cannot pull out the padlocking tab, the chassis can be locked in disconnected position only. Execute the locking procedure then the unlocking procedure.
-
If you can pull out the padlocking tab, the chassis can be locked in disconnected, test, or connected position. The locking and unlocking procedures are the same as with chassis in disconnected position. Execute these procedures in each position: connected, test, disconnected.
The following table shows the chassis locking configurations.
|
Chassis locking system |
Device position in the chassis |
Padlocking tab |
Racking handle insertion with chassis locked |
|---|---|---|---|
|
Chassis locking in disconnected position |
Connected |
Cannot be pulled out |
Possible |
|
Test |
Cannot be pulled out |
Possible |
|
|
Disconnected |
Can be pulled out |
Not possible |
|
|
Chassis locking in any position |
Connected |
Can be pulled out |
Not possible |
|
Test |
Can be pulled out |
Not possible |
|
|
Disconnected |
Can be pulled out |
Not possible |
Checking Chassis Padlocking With Device in Disconnected Position
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Verify that the racking handle is not inserted in the racking handle socket. |
|
|
2 |
Pull out the padlocking tab. |
If the padlocking tab cannot be pulled out, contact your Schneider Electric Services representative. |
|
3 |
Insert the padlock in this tab. |
|
|
4 |
Check that the racking handle cannot be inserted into the racking handle socket. |
If the racking handle can be inserted, contact your Schneider Electric Services representative. |
Checking Chassis Unlocking With Device in Disconnected Position
Before starting this check, verify that the chassis is locked in disconnected position.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Remove the padlock from the tab.
|
If the tab does not retract fully, contact your Schneider Electric Services representative. |
|
2 |
Check that the racking handle can be inserted into the racking handle socket so that racking operations can be carried out. |
If the racking handle cannot be inserted, contact your Schneider Electric Services representative. |
DANGER