Mechanism NIII_Z_2: Check the General Condition of the Mechanism
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF DEVICE FALLING
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check the general condition of the mechanism:
|
|
Goal |
Verify that the mechanism correctly opens and closes the device. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
Torx screwdriver |
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Removed from chassis |
Removing Front Cover
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
For MasterPacT MTZ1: Remove the spring charging handle. |
|
|
2 |
Remove the front cover of the device. |
Checking Cable Between the ULP Port Module and MicroLogic X Control Unit
If you have installed the ULP port module, follow the procedure described below:
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check that the wire is not damaged and is correctly positioned so that it does not interfere with the reset mechanism. |
If the wire is damaged, replace it. Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. |
|
2 |
Check the cable connection to the MicroLogic X control unit. |
If the connection is loose, reinsert the cable, making sure that the connector is fully inserted. |
Checking Mechanism
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Remove the mechanism cover:
|
If the mechanism cover is damaged, contact your Schneider Electric Services representative. |
|
2 |
Check the general condition of the mechanism:
|
If there is dust on the mechanism, or the consistency or color of the grease has changed, contact your Schneider Electric Services representative. |
|
3 |
If necessary, reposition the voltage releases (refer to MasterPacT MTZ - MN-MX-XF Voltage Releases - Instruction Sheet). |
|
|
4 |
Check that the springs are present, in good condition, and correctly positioned in the groove on the axle.
|
If a spring is damaged or missing, contact your Schneider Electric Services representative. |
|
5 |
Manually charge the mechanism. |
|
|
6 |
Check that the springs are correctly positioned. |
If a spring is not correctly positioned, carefully put it back into place. If the problem persists, contact your Schneider Electric Services representative. |
|
7 |
Close the device. |
|
|
8 |
Check that the springs are still correctly positioned. |
If a spring is not correctly positioned, carefully put it back into place. If the problem persists, contact your Schneider Electric Services representative. |
|
9 |
Check the number of operating cycles and compare it with the maximum allowed for the connecting-rod springs as indicated in MasterPacT MTZ - IEC Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Unit - Maintenance Guide . |
If the maximum number has been reached, contact your Schneider Electric Services representative. |
|
10 |
Put the mechanism cover back in place. |
Reinstalling the Front Cover
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Put the front cover back in place. |
|
|
2 |
For MasterPacT MTZ1: Put the rubber cover back in place on the spring charging handle. |
DANGER
DANGER