Customizing the Toolbars

  1. From the Tools menu, select Customize, or right-click in the toolbar area and select Customize.

    The Customize window opens.

  2. Select the Commands tab.
  3. Click and drag the Command item from the Customize window to the toolbar. A black vertical line appears in the toolbar indicating the new button position.
  4. Repeat as needed.
    NOTE: To remove buttons, click and drag the button off the toolbar while the Customize window is open.
  5. When you are finished customizing, click Close.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.