Switching Orders and Templates

Switching orders must be deleted from the Switching Order Library.

  1. In Responder Explorer, select File > Switching Orders.
  2. Click Open a Switching Order or Template from the Library. This displays the Switching Order Library.
  3. In the Switching Order Library, right-click the switching order or template that you want to delete, and then select Delete.
  4. You are prompted to confirm deletion of the selected object. Click Yes to delete or No to return to the Switching Order Library without deleting.
  5. Close the Switching Order Library.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.