Add Snippet to Switching Order

When you add a snippet to a switching order, remember that it is added after the operation that you have selected. If you have no operations in the switching order, you can simply double-click the snippet to add it. If you have operations already in the switching order, select the operation after which you want the snippet added. If you select the first operation in the switching order, you can then double-click a snippet. The operations in the snippet are added after the first operation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.