Create Snippet

To create a snippet, add the operations that you want to save to the switching order. Select the operations, and then select Create Snippet in the Order menu. All selected operations are saved to the snippet exactly as they are. If you have assigned a device to an operation, it is assigned in the snippet as well. You need to select a category for the snippet, and to provide it with a name and description. The description text is visible when the snippet is selected on the Snippets tab.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.