Prediction

If a fault is placed at SP1, SP2, or SP3, the Prediction Engine considers the next upstream device, which in this case is T1. If the fault is determined to be further upstream than T1, the Prediction Engine moves to the next upstream device, which is the fuse. The Prediction Engine can create a fault on the fuse, but not on anything upstream because it would have to guess at which upstream path to choose.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.