Create a Template

Available in Responder Explorer.

Follow these steps to create a switching order template.

  1. In Responder Explorer, select File > Switching Orders.
  2. Click Create a Template. This displays the Select Location & Name screen.
  3. In the Select Location & Name window, browse to the location in the Switching Order Library where you want to store the template.
  4. In the field at the bottom of the screen, type a name for your template. Click OK.
  5. Use the Switching Order Editor to edit the new template.
  6. When you've finished editing the operations, click Save from the Order menu and close the window.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.