Attribute Viewer

When the user performs a search, an identify, or any task that selects features on the map, results are displayed on the Attribute Viewer. In the example below, the selected service point features are highlighted in blue on the map and displayed in the Attribute Viewer at the bottom of the window.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.