Move Up

If a problem is reported with T1 and a crew determines that T1 is not at fault, you can move the fault to the next unconfirmed upstream device. If Responder encounters a split when moving to the next upstream device, Responder is unable to determine which feeder is at fault.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.