Create Tag
Available in ArcMap.
This tool allows you to place a tag on a device without a switching order or an incident. If a tag is placed on a device that is already part of an incident, the device is automatically confirmed. Tags can be placed only on features that participate in the geometric network.
-
Click the Create Tag
button
on the Responder toolbar.
The cursor becomes a circle with a blue dot in the middle. The blue dot snaps to all selectable devices. A layer must be set as selectable before this tool snaps to its features. - Click a device on the map.
- Type the tag information in the Create Tag window.
-
Click OK.
If a tag with the same name already exists on the selected feature, the user receives a warning. However, tags with identical names can still be created.
The tag can be viewed in Responder Explorer on the Tags tab.
NOTE: ‘Do Not Energize’ is the only available tag type for conductors. Other operational tags make sense only for operable/point features.