Change Hazard

Available in Responder Explorer.

Change Hazard allows you to move the location of a hazard, regardless of whether its status is confirmed or unconfirmed. The hazard is removed from the original feature and replaced on the feature specified by the user.

  1. Right-click a hazard and select Change Hazard.

    In ArcMap, the cursor changes to the following:

  2. Click a feature to replace the feature currently selected in the incident.
  3. You can modify the following fields on the Edit Hazard window: Hazard Type, Wire Owner, Remarks, and the Public Safety fields.
  4. Click OK to save changes and close the form.

    Changing a fault may affect prediction.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.