Create a Switching Order or Template in Switching Order Library

Available in Responder Explorer.

If you have the Switching Order Library open and want to create a new switching order or template, you can do so without needing to close the library. Simply right-click a directory and select New > Switching Order or New > Template. The new switching order or template is created in the directory that you right-clicked. It is also opened for editing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.