Save as Template

Available in Responder Explorer.

Alternatively, you can save an open switching order as a template. Follow these steps:

  1. Open a switching order.
  2. Use the Switching Order Editor to edit as needed.
  3. In the Switching Order Editor, select Order > Save as Template. This displays the Select Location & Name screen.
  4. In the Select Location & Name window, browse to the location in the Switching Order Library where you want to store the template.
  5. In the field at the bottom of the screen, type a name for your switching order. Click OK.
  6. When you've finished editing the operations, click Save from the Order menu and close the window.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.