Devices Tab

Available in Responder Explorer.

All electric devices assigned to open incidents are displayed on the Devices tab in Responder Explorer. You can highlight any device in the list and select from tools to view it in the map (Highlight, Zoom To, Pan To, Quick Attribute Viewer). You can also right-click any device and select Show in Incident Grid to locate the incident with that device on the Incidents tab.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.