Auto-Confirm

In a multifeed situation, if you create a fault at switch S1, it is auto-confirmed because multiple feedpaths exist both upstream and downstream of a device. If there is a fault on the fuse or any downstream device, it is not auto-confirmed because at least one side of the device has only one feedpath.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.