Display

The Attribute Viewer displays layers on separate tabs. Each tab is marked with a different color to help identify those features on the map. In the example above, the Service Point tab is selected and the identified service points are displayed in the map. Should the user select the Transformer tab, the map display would change to display only the identified transformer, and it would be highlighted in red. Any feature selected in the Attribute Viewer is highlighted in white on the map.

You can view additional information about selected features and related objects using the Attribute Details tool.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.