Reports Tab

Select the Reports tab to generate a number of available reports. Before running Reliability Reports for the first time, you must execute the Update Population Information tool (discussed on the Responder Toolbar in ArcMap page). This populates a field in the Archive tables with the total number of customers. You can execute this tool to update the customer count before executing subsequent Reliability Reports.

To execute a report, select it in the list on the left, provide the required information on the right, select an Output type, and then click Generate. The Output field allows you to display the report in a web browser or in an Excel spreadsheet. The report is displayed in a separate web browser window. If you're executing a report that requires a date range, Archive Explorer sets the incident Outage Time equal to the incident Creation Time if the Outage Time field is empty.

NOTE: The weeks in the biweekly Reliability reports begin on the same day of the week as the start date for the reporting period. For example, to have weeks begin on Monday, ensure that the start date for the reporting period falls on a Monday.
IMPORTANT: The Reliability Indices do not include planned outages. You can include planned outages by performing an optional configuration outlined in the Configuration Guide.

The Reports tab includes the following:

You may have custom reports in your list that were created by your Admin which won’t be listed below. Please see your Admin for additional details about those custom reports.

Report

Description

Incidents by ID

A detailed report for the incident for an incident ID.

Incidents by Date Range

A tabular report of incidents with outage time within a date range.

Incidents by Duration

A tabular report of incidents within a specified date range with a minimum or maximum duration.

Incidents by Feeder

A tabular report of incidents within a specified date range that occurred on a feeder.

Incidents by Customer

A tabular report of incidents within a specified date range experienced by a customer.

Incidents by Device Type

A tabular report of incidents within a specified date range that occurred for a device type.

Incidents by Devices

A tabular report of incidents within a specified date range that occurred for a device.

Critical Incidents

A tabular report of critical incidents within a specified date range.

Devices with Multiple Outages

A report of devices that have experienced more than one outage within a specified date range.

Operations on DPDs (duration <= 1 min)

A report of incidents involving operations on Dynamic Protective Devices lasting no more than one minute within a specified date range.

Operations on DPDs - Summary

A summary report by feeder of incidents involving operations on Dynamic Protective Devices within a specified date range.

Outages (duration >= 1 min)

A report of incidents involving outages with customers lasting one minute or more within a specified date range.

Outages - Summary

A summary report by feeder of incidents involving outages with customers lasting one minute or more within a specified date range.

Customer Counts by Feeder

A report of customer counts by feeder, based on the count made on the date closest to the selected date.

Reliability Indices - System-wide

A tabular report of reliability indices for the entire network, which can be listed by year, month, week, day or to date.

Reliability Indices - Selected Feeder

A tabular report of reliability indices for the specified feeder, which can be listed by year, month, week, day or to date.

Reliability Indices - By Feeder

A tabular report of reliability indices for the entire network, broken down by feeder, which can be listed by year, month, week, day or to date.

Reliability Indices - SAIDI By Cause Code

A tabular report of reliability indices for the entire network, broken down by cause code and listed by SAIDI. By default, this report does not exclude Planned Outage and Non-Outage cause codes. Your administrator can configure this report to exclude the unnecessary cause codes.

Reliability Indices - SAIDI By Cause Code - Summary

A tabular report of reliability indices for the entire network, broken down by categories defined by your administrator, as a summary. This report's default configuration is set for those utilities utilizing the RUS Cause Code domain.

Minutes and Outage Count by Cause Code

A tabular report showing the number of outages and number of minutes interrupted by cause code within a specified date range. By default, this report does not exclude Planned Outage and Non-Outage cause codes. Your administrator can configure this report to exclude the unnecessary cause codes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.