Delete Snippet

To delete an existing snippet or snippet category, right-click it on the Snippets tab and select Delete Snippet. You are then prompted to confirm that you want to delete the selected snippet or category. Click Yes to delete or No to cancel without deleting.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.