Add Operation

  1. Type the new operation in the New Operation field. We recommend that the operation consist of the Responder table and the operation that can be performed (e.g., insert, select, update, delete). For example: RX_CREWS,DELETE.
  2. Click Create.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.