Add Hazard on Incident Device

Available in Responder Explorer.

This tool allows you indicate a hazard on an electric device assigned to an incident. An electric device can have multiple hazards.

  1. Right-click an electric device and select Add Hazard.
    The Edit New Hazard dialog displays information about the hazard.
  2. Modify the Hazard Type and Wire Owner as needed.
    NOTE: Only fields displayed in white can be edited.
  3. If public safety officers have arrived at the scene, enter their arrival time in the Time of Arrival field of the Public Safety section; after the hazard has been eliminated, enter their departure time into the Time of Departure field.
  4. Type any additional pertinent information about the hazard into the Remarks text box.
  5. Click OK to add the hazard to the selected incident in Responder Explorer.
    NOTE: Multiple hazards can be added to a single incident device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.