Responder Multifeeds

While Responder does support multifeeds, there are scenarios in which multifeeds are not supported. The following diagram illustrates the ways in which multifeeds are not fully supported:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.