Tabular

This tab displays data in a tabular format. Select the data that you want to view from the drop-down menu.

  • Customer Status: This data displays the number of customers in each region and the number impacted by an outage.

  • Interruption Status: This data displays the number of interruptions in each region and data about the number of interruptions with crews assigned.

  • Crew Status: This data displays the total number of crews and the percentage assigned to incidents and hazards.

  • Hazards Status: This data displays the number of hazards and the percentage assigned to crews.

  • Calls Status: Displays the number of active calls in the system and the number of unassigned calls.

  • Region Estimated Time of Restoration: Shows the estimated time of restoration for the selected region. If you have selected a region that contains other regions, the estimated times of restoration are displayed for each sub-region. This value reflects the estimated time of restoration set on the Restoration Estimates page in the Dispatchers section.

  • Feeder Estimated Time of Restoration: Shows the estimated times of restoration for the feeders in the selected region. These values reflect the estimated times of restoration set on the Restoration Estimates page.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.