Analytical

This tab displays several types of information in the form of graphs. The information shown is for the region selected on the left.

  • Customer Status: The percentage reflects the amount of customers affected by any type of incident.

  • Interruption Status: The percentage reflects the number of interruptions with no crew assigned.

  • Crew Status: This data displays the total number of crews and the percentage assigned to incidents and hazards.

  • Hazards Status: This data displays the number of hazards and the percentage assigned to crews.

  • Call Status: This portion displays the status of incoming calls, such as the number of active calls and the number that have not been restored within 30 minutes.

  • Outage Cost: Displays the dollar amount of revenue lost due to the current outages.

  • Estimated Time of Restoration: Displays the estimated time of restoration for the selected region. This reflects the estimated time of restoration set on the Restoration Estimates page in the Dispatchers section.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.