Make Lead Crew

Available in Responder Explorer.

If multiple crews are assigned to the same incident, you can designate one crew as the lead crew.

NOTE:  The Lead Crew is the crew that shows up in the calculated column that is visible at the incident level.
  1. Right-click a crew and select Make Lead Crew.
  2. The crew's Lead Crew? field now has a value of Yes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.