Query Incidents

After selecting the Incidents tab, the Query tool allows you to filter through all the data. Select a query from the list, choose the parameters, and then click OK.

  • Incidents by Date Range: Display all incidents that occur within a specific date range, based on the date and time of their creation.

  • Incidents by Region: Display all incidents within a specific region or multiple regions that occurred within the Outage Date and Time range.

  • Incidents by Feeder: Provide a valid Feeder ID to display all incidents that reside on a specific feeder and occurred within the Outage Date and Time range.

  • Incidents by Device Type: Query the database for incidents with a specific type of device that occurred within the Outage Date and Time range.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.