Available Operations

The following operations are available by default in Responder Web Browser. They can be assigned to tasks as needed.

Operation

Description

APPROVE_SWITCHING_ORDER

This operation allows users to approve a switch order.

ARCHIVE_MASS_EDIT

This operation allows users to edit multiple loadpoints or calls of an archived incident at one time.

ARCHIVE_REPORTS

This operation allows users to run Archive Reports on the Web.

CALL_ALLOW_EDIT_TIME_OF_OUTAGE

This operation allows users to edit the time of call on the web page (if configured to do so).

CANCEL_SW_OR_REQUESTS

This operation allows users to cancel switch order requests that they do not own.

CHANGE_NORMAL_STATE

This operation allows users to use the change normal state tool.

CREATE_SWITCHING_ORDER, DELETE_SWITCHING_ORDER, EDIT_SWITCHING_ORDER

This operation allows users to create, delete, and edit switch orders.

CUSTOM_REPORT_DELETE, CUSTOM_REPORT_SAVE

This operation allows users to create and delete custom reports.

DELETE_ARCHIVED_INCIDENTS

This operation allows users to delete incidents, calls, or loadpoints from the Responder Archive Explorer.

DISPATCHER_SELECTABLE

This operation allows dispatchers to be listed as dispatchers in explorer.

EDIT_SW_OR_REQUESTS

This operation allows users to edit switch orders that are owned by other users.

EDIT_SWITCHING_ORDER_IN_EXECUTION

This operation allows users to edit a switch order that is currently in execution.

EXECUTE_SWITCHING_ORDER

This operation allows users to execute a step on a switch order.

INCIDENT_REVIEW

This operation allows a user to use the Incident Review tool.

LINE_DISPLAY_REPROCESS_ALL

This operation allows users to remove and reprocess the current line display and jumpers in ArcMap.

NOTE: With this permission you can reprocess the line display and jumpers for all incidents, regardless of whether you are the dispatcher for that incident. Without this permission, you can only reprocess the line display and jumpers for the incidents in which you are the dispatcher.

LONG_TERM_DEVICE

This operation allows users to make a device long term.

MODIFY_FOLDER_STRUCTURE

This operation allows users to change the folder structure in the library (create, move, delete folders).

MODIFY_TASK_SNIPPETS

This operation allows users to create/modify snippets.

PLACE_JUMPER

This operation allows users to place a jumper from ArcMap or within Responder Explorer.

PLAN_SWITCHING_ORDER

This operation allows users to plan a switch order (setting the start/finish time).

REMOVE_JUMPER

This operation allows users to remove jumpers from ArcMap and Responder Explorer.

REPROCESS_DEVICES

This operation allows users to reprocess devices on an incident, updating loadpoints and outage times.

RX_CALLS,DELETE

This operation is an example of a table-based permission to delete.

RX_CALLS,INSERT

This operation is an example of a table-based permission to insert.

RX_CALLS,SELECT

This operation is an example of a table-based permission to select.

RX_CALLS,UPDATE

This operation is an example of a table-based permission to update.

SAVE_SWITCHING_SIMULATION

This operation allows users to save switch order simulation results to the database.

SELECTABLE_FOR_EXECUTE_BY

This operation displays the dispatcher in the dispatcher drop-down for executing steps on a switch order.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.