Edit Electric Feature Operations

Archive Explorer offers two ways to access and edit information about electric features associated with an incident.

  • From the Edit Incident window, right-click an electric feature on the Electric Features tab and select Edit. The Electric Features tab displays all electric network features associated with the incident. Multiple rows can exist for a single feature. This displays each operation on the feature (e.g., confirm, resolve).

  • On the Archive Explorer Incident tab, expand the incident to display the electric features associated with it. Multiple rows can appear for a single feature. Each row represents an operation on that device.

When you right-click and select Edit on an electric feature operation (in either location), the following Edit window appears. You can edit feature information such as the number of Customers impacted, the Actual Status, Region, Time of Operation, Device Operation, and Confirmed status. Fields in gray cannot be edited. The Highlight, Zoom To, and Pan To tools are enabled only if you have ArcMap open.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.