Run the Customer Count by Feeder Report

The Generate Reports tool allows you to create various types of customer reports independent of an incident. You can display a list of customers grouped by feeder.

  1. In Responder Explorer, click the Generate Reports button.

    The Reports window opens.

  2. Select a Report Type of Customer Count By Feeder.
  3. Select one of the following Output types:
    • Excel: Creates an Excel spreadsheet (.xls).

      NOTE: If you select Excel and are creating multiple reports, you must close the previous report (or save it with another file name) before creating another.
    • Browser: Creates an HTML page.

  4. Click Generate to create the report.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.