Request

This tab displays information about a switching order request assigned to the switching order. This data cannot be edited in the Switching Order Editor. You can right-click a device in the Requested Devices list and select a tool: Zoom To, Pan To, Highlight, Highlight Steps, or Assign Device. The Assign Device tool assigns the device to the selected operation. If the selected operation already has a device assigned, it is removed and replaced with the requested device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.