Tasks

Available in Responder Explorer.

The Tasks (or operations) are listed on the left side of the Switching Order window. This section displays all tasks (or operations) that are available to assign to your switching order. If you select a task on this pane, a description of it appears in the window below the tasks ('Open Device' in the example below).

Double-click or drag tasks from the Tasks tab to the window on the right to add them to the switching order.

IMPORTANT: A tag that was created outside of the switch order can be removed only if the Network State is set to Current State. Modify this setting by selecting Order > Network State in the Main menu. The Network State setting is displayed in the bottom right corner of the Switching Order Editor.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.