Scheduled Switching Order

You can edit a switching order that has been scheduled to execute at a later date.

  1. In Responder Explorer, select the Scheduled Switching Orders tab.
  2. Right-click the switching order you want to edit, and then select Edit.
  3. Use the Switching Order Editor to edit as needed.
  4. When you're finished editing the operations, click Save from the Order menu and close the window.
    NOTE: If you click the red X in the window's upper-right corner, the entire window closes, along with any other switching orders in the window. If changes have been made to any switching order, a prompt appears for you to save the changes for each order.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.