Related Objects

If a related object exists and has been properly configured, it can be displayed in the Attribute Viewer. In the example above, the second Service Point is expanded to show the related customer information. If the related object has spatial representation on the map (i.e., shape), you can pan or zoom to it. For example, a pole may be related to a transformer. Hover the cursor over the first field in the related object row to display the Pan and Zoom tools.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.