Amplifier Internal Equalizers Properties

Amplifier Internal Equalizers.

Equalizer Value in dB (required)

The auto-optimization engine uses this value in calculations for optimizing your network design in Designer HFC.

Equalizer Type (required)

Select Forward or Return from the drop-down list.

Insertion Loss (required)

Loss of signal strength at the insertion point.

  • Remove: Click the Remove button to the right of the value that you want to delete.

  • Add: Type the appropriate value(s) and click the Add button to the right of the value(s) you are adding.

  • Edit an existing value: Double-click the existing value and type a new value, then click Update to save all changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?