Taps Leg

Remove: Click the Remove button to the right of the value that you want to delete.

Add: Type the appropriate value(s) and click the Add button to the right of the value(s) you are adding.

Edit an existing value: Double-click the existing value and type a new value, then click Update to save all changes.

  • Forward Tap Loss (required) : The amount of forward tap loss at particular frequencies.

  • Return Tap Loss (required): The amount of return tap loss at particular frequencies.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?