Segmentable Nodes Supported Segmentations
Check the boxes to enable:
-
Non Segmented
-
Two Way
-
Three Way
-
Four Way
In the application, the options you check are presented to the end user when viewing the node’s properties:
For each segmentation, specify the Power Profile, as needed.
Power Profile (required)
The power profiles are available for the different segmentation configurations that are selected in the Supported Segmentations section. Different segmentations have different powering draws, so you have the ability to specify the consumption for each segmentation.
-
Remove: Click the Remove button to the right of the value that you want to delete.
-
Add: Type the appropriate value(s) and click the Add button to the right of the value(s) you are adding.
-
Edit an existing value: Double-click the existing value and type a new value, then click Update to save all changes.