Amplifiers Details
Manufacturer
The manufacturer of the component.
Model Number (required)
The component's model number. The model number is required to be unique across all resources of the same type.
Company ID
The ID your company assigns to the component. It is recommended that you use unique company IDs. You will see a warning if you type a company ID that is not unique, but you are allowed to continue with a non-unique ID.
Amplifier Type (required)
In this drop-down box you can assign the type of amplifier that you want in your design. Select either Line Extender or Mini-Bridger.
Description
A short description of the component.
GIS Symbology
GIS Symbology provides you with the ability to specify symbology text for various component specifications in Catalog. This text is published to GIS with DHFC features and can be used as a basis for symbology.
Catalog Id
The GUID assigned to the component.
Is Deprecated (default: not selected)
Toggle to mark the component as deprecated.