Supported Amplifier Profile Configurations

Specific profile configurations are supported by the application. In cases where Amplifiers have invalid profile configurations, the Swap button is disabled for internal plugins in the DHFC application.

The maximum number of outputs allowed is 5. The application prevents you from adding more than 5.

Supported configurations include:

  1. Having 1, 2, or 3 forward profiles with no internal coupler enabled on any of the profile configurations.

  2. Having 1 profile configuration with internal coupler enabled (net result of this is 2 outputs in DHFC).

    IMPORTANT: If you enable internal couplers for at least one profile, you must have Splitters or Directional Couplers in the Forward Internals. If you do not have these, you cannot save the amplifier.

  3. Having 2 profile configurations with internal couplers enabled. Valid combinations include:

    1. Having 1 profile configuration with internal coupler disabled and 1 port configuration with internal coupler enabled (net result of this is 3 outputs in DHFC).

    2. Having 2 profile configurations with both having the internal coupler enabled (net result of this is 4 outputs in DHFC)

  4. Having 3 profile configurations with internal couplers enabled. Valid combinations include:

    1. Having 2 profile configurations with internal coupler disabled and 1 port configuration with internal coupler enabled (net result of this is 4 outputs in DHFC).

    2. Having 1 profile configuration with internal coupler disabled and 2 port configurations with internal coupler enabled (net result of this is 5 outputs in DHFC).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?