Plugins

If you’ve already configured conditioning taps, then you know that certain components require plugins, which are defined as additional devices built into the main component. Refer to the Plugins topic under Conditioning Taps for information about adding plugins..

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?