Inline Equalizers Details

Inline Equalizers

Manufacturer

The manufacturer of the component.

Model Number (required)

The component's model number. The model number is required to be unique across all resources of the same type.

Company ID

The ID your company assigns to the component. It is recommended that you use unique company IDs. You will see a warning if you type a company ID that is not unique, but you are allowed to continue with a non-unique ID.

Description

A short description of the component.

GIS Symbology

GIS Symbology provides you with the ability to specify symbology text for various component specifications in Catalog. This text is published to GIS with DHFC features and can be used as a basis for symbology.

Catalog Id

The GUID assigned to the component.

Is Deprecated (default: not selected)

Toggle to mark the component as deprecated.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?