Inline Equalizers (LEQ/RC) Properties

Inline Equalizer LEQ/RC

Point Size (required)

Assign a point value to a component based on physical size. With a consistent point value system you will be able to determine how much equipment can fit inside an enclosure. For example, if you have a pedestal rated to hold 30 points worth of components, then you can situate three 2-port taps rated at 10 points each into the box. A fourth 2-port tap would total 40 points, exceeding the rated 30 points of the pedestal.

Maximum Amperage

The amps that the manufacturer rates as maximum for the node.

Forward Loss (required): The amount of forward signal loss at a particular frequency.

Forward Bypass Loss (required): The amount of forward bypass signal loss at a particular frequency.

Return Loss (required): The amount of return signal loss at a particular frequency.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?