ArcFM Connectivity Evaluator (ACE) Tool
The ArcFM Connectivity Evaluator (ACE) tool is a separate application from and Solution Center. Its core function is to test and verify connectivity to ArcFM services and, depending on the application, connectivity to Azure Service Bus. This is a crucial prerequisite before performing Solution Center configuration or any plugin configuration, as you need connectivity for the configuration to work.
When using the ACE tool, keep the following in mind:
-
The tool’s purpose is testing connectivity, so it only works after your company’s tenant is created.
-
The tool can be run as many times as needed until all issues are corrected. This is particularly helpful throughout the implementation process.
-
The ACE installer can be downloaded from the ArcFM Solution Center article on myArcFM. You must have a myArcFM account and be logged in to download files.
-
Install and run the ACE tool on the same machine that runs the ArcFM application you are testing.