DOCA0221EN-01

Locking the Door

Before starting the procedure, check that the device is in the disconnected position.

Step

Action

1

Close the door.

2

Turn the racking handle until the device is in test or connected position.

3

The door is locked.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.