DOCA0221EN-01

Locking the Switchboard Door

Description

The locking option is installed on the left or right-hand side of the chassis:

  • When the device is in connected or test position, the latch is lowered and the door is locked.

  • When the device is in disconnected position, the latch is raised and the door is unlocked.

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: 51201014AA.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.