DOCA0221EN-01

Favorable Conditions For Device Installed Inside a Switchboard

The time interval between two preventive maintenance visits can be doubled if all the conditions presented below are met.

The only exception is the check-up program recommended for the fifth year.

Favorable operating and environmental conditions for device installed inside a switchboard

Temperature

Average annual temperature <25 °C (77 °F) outside the switchboard (Ti*). The device is installed in an air-conditioned room or in a ventilated enclosure.

Percent load

< 50% of In 8/24 hours or 24/24 hours

Relative humidity

< 50%

Corrosive atmosphere

Device installed in environment category 3C1 or in a closed room that creates favorable conditions (air is conditioned and purified)

Salt environment

None

Dust

Negligible

Device installed in a switchboard equipped with filters or a ventilated IP54 enclosure

Vibration

None

Example depending on the conditions:

  • Normal: check on charging time = 2 years

  • Favorable: check on charging time = 2 x 2 = 4 years

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.