DOCA0221EN-01

Locking in the Disconnected Position

Combination of Locking Systems

It is possible to lock the device on the chassis in the disconnected position using:

  • One to three padlocks (standard feature)

  • One or two keylocks (optional feature)

  • A combination of both.

NOTE: If specified when ordering the chassis, this locking function may be adapted to operate in all positions (connected, test, and disconnected), instead of in disconnected position alone.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.