DOCA0221EN-01

Locking the Toggle Handle in the ON or OFF Position

You can use one to three padlocks (shackle diameter 5 to 8 mm (0.2 to 0.3 in)) to lock the toggle handle in the ON or OFF position.

NOTE: The circuit breaker trips even when locked in the ON position.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?