DOCA0221EN-01

Remote Opening

Use either:

  • An MX opening voltage release.

  • An MN undervoltage release.

  • A delayed MN undervoltage release.

When connected to the control panel, these releases may be used to remotely open the device.

MX, MN

MN delay unit

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?