DOCA0221EN-01

Maintaining the Communication System

Via the communication network, the communication module transmits data to a remote site for use by various departments (for example, maintenance, management, production). A break in the transmission of data can result in:

  • Production losses due to unawareness of the status of the device

  • Financial losses due to incorrect system management

  • Diagnostic errors

Periodic checks on the orders (read, write, commands) transmitted by the communication network are required to maintain a high degree of reliability and confidence in the communication system.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.